Develop an archives manager
Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
TIP:
You can download a sample project from:
ExampleApplication-ArchivesManager.zipPrerequisites
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Provide Feedback