Develop a solution for importing UI from another project
Use OPC UA communication to import the UI from another project and display the values of selected variables.
NOTE:
Download a sample project:
ExampleApplication-ImportUI.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
TIP:
The Client project will import data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
In
FactoryTalk Optix Studio
, select to run Server and Client projects using the client emulator to test your project. To run the project on a remote client, see Add a client device.Provide Feedback