Configure a static network
Configure a static network by adding a system object and configuring its parameters.
- Create a system object instance:
- InType view, double-clickSystem.
- DragSystemfromType viewtoModelinProject view.At runtime,FactoryTalk Optix Studiocreates an object for each network interface (wired) detected on the machine.
- InFactoryTalk Optix Studio, select to run the project using the client emulator to test your project. To run the project on a remote client, see #.
- At runtime, set the relevant values.TIP: In case of a configuration error,FactoryTalk Optix Studioshows an error message in the FTOptixRuntime log.
Restart the machine to complete the configuration.
TIP:
If the DHCP service is active within the System object, the addresses automatically assigned by the DHCP server are saved.
Provide Feedback