Create a project
A project contains elements with which a
FactoryTalk Optix Application
is made.- From the main menu, selectNew HMI project.
- Select the project template:
- ChooseDefaultto use a pre-configured project template.
- ChooseBlankto create and configure all project components manually.
- Set the projectNameandLocation.
- (optional) SelectUse version controlif want to version your project with Git.
- SelectCreate.
The new project opens.
Provide Feedback