Create a template from an object or variable
Use a template to create other objects and variables that have similar attributes. Create a template by dragging an object, variable of an object, or variable from
Template
Libraries
into a folder in Project
view
.- SelectTemplateLibraries.
- FromProjectview, drag the desired object or variable into a library inTemplateLibraries.
- (optional) Enter a description of the template. Select the template inTemplateLibraries, in the box below the library contents type the description, and then selectClose.
Provide Feedback