Monitor the value of a server variable

Use the UaExpert® client to monitor the values of server variables and set the value update interval. Monitoring the values of server variables is useful for debugging.
  1. From
    Address Space
    , drag a variable to the
    Data Access View
    pane.
    The line displays the updated value in real time and a time stamp.
  2. To perform advanced actions (for example, to set the update interval value update, in
    Data Access View
    ), right-click the variable and select an option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.