Navigate the server project information model
Use the UaExpert client to navigate the information model of the server project. Navigating the information model is useful for verifying which nodes are published.
Prerequisites
- InAddress Space, navigate to to expand the root node of theFactoryTalk Optix StudioOPC UA server project.
The node is displayed as a folder with the same name as the project. The published project nodes are available.
Provide Feedback