ASEM EtherNet/IP Station

ASEM EtherNet/IP Station

Object that represents a controller that communicates via the ASEM EtherNet/IP protocol.
BrowseName
EthernetIPStation
SuperType
Communication station(CommunicationStation)

Properties

Name
BrowseName
DataType
Description
Maximum job size in bytes
MaximumJobSizeInBytes
Maximum size in bytes of a transmission of tags from the controller. 0 = 504 bytes (maximum value).
IP Address/Slot (optional)
IPAddress
Unique address of the controller on the network. The slot can be specified for ControlLogix control systems (for example, 192.168.1.10/1:1).
Port
Port
Number of the port used by the TCP-IP connection. It must match the one configured in the controller.
Timeout
Timeout
Maximum wait time in milliseconds to receive a response from the controller.
Physical Address Optimization
PhysicalAddressOptimization
Physical Addressing Optimization (used only with Tag Name addressing). If True, the driver gets for each controller tag its physical (internal) address and use it in read requests, instead of the variable name. When many tags with long names must be read, the use of physical addresses can considerably improve the refresh rate of the tags. If True, it requires an initialization phase to translate the variable names into physical addresses, this means that greater is the number of variables on the controller, the longer the initialization phase is. Once the physical address initialization is completed, the seventh bit of the State/Command Variable is set to 1
Operation code
OperationCode
(Inherited from Communication station)
Tags
(Inherited from Communication station)
Types
(Inherited from Communication station)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal