- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Move a graphic object
Move a graphic object in the window to position objects as they will appear at runtime. All of the objects in a container move with the container.
- To move a graphic object either:
- In the window, select and drag the container or graphic object.
- InProject view, select the container or graphic object and then inPropertieschange:
- Horizontal alignment. Enter the value for the space between the object and the X-axis.
- Vertical alignment.Enter the value for the space between the object and the Y-axis.
TIP: The position of the graphic object inProject viewdetermines the order of graphic objects on the Z-axis compared to other objects in the same container. Objects lower in the tree appear higher in the order on the Z-axis.
Provide Feedback