- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Configure Custom Payload
- In Project View, select the MQTT Publisher you want to modify.
- In the properties, underPayload formatter:
- SetPF EnabledtoTrue.Payload Formatter is enabled.
- Next to thePF Header, select the dynamic link.
- In the new window, in theAdvancedtab, define the header string format, and selectCreate.
- Next to thePF Record, select the dynamic link.
- In the new window, in theAdvancedtab, define the record string format, and selectCreate.TIP: If you do not have any records, you can leave thePF Recordblank.
Provide Feedback