- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Delete a node
Delete a node to remove it from the project. Deleting a node removes any references to other nodes. If the deleted node references other nodes, you are prompted to remove all of the references to other nodes.
- InProject view, select the node.
- In the view toolbar, select.Delete
- If the node references other nodes, a list of the referenced nodes appears. SelectDeleteto confirm the deletion.
Provide Feedback