- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Sessions and users in C#
Read and modify the properties of a runtime session through the properties of the Session C# variable, displayed by NetLogic. Modify session properties to authenticate another user for a session or change the locale of the session.
To read or modify the session properties, see Read or modify the session properties.
Provide Feedback