- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a database
Create a database for the event logger.
- InProject view, right-clickLoggersand select .
- Add a database table with the following columns:Column nameTypeValueActiveState_IdBooleanFalseAckedState_IdBooleanFalseConfirmedState_IdBooleanFalseTimeUtcTimeNot setMessage_it-ITStringMessage_en-USStringSeverityUInt160For more information, see Configure a database table.
Provide Feedback