- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create an alarm
Create an exclusive level alarm that warns about exceeded temperature.
- InProject view, right-clickAlarmsand select .
- InProperties, setHigh limitto60.
- SetAuto confirmtoTrue
- SetMessagetoMaximum temperature exceeded
- Create a dynamic link betweenInput variableand .For more information about dynamic links, see Create dynamic links.
Provide Feedback