Ladder or Structured Text Font and Color Preferences
Set font and color preferences for the
Logix Designer
application in the Workstation Options
and Print Options
dialog boxes. Workstation Options
contains settings for display on the screen, and Print Options
contains settings that control the appearance of printed reports. Display and printing preferences can be configured differently, even though the options for the Font/Color
categories are same on each dialog box.
TIP:
- To open thePrint Optionsdialog box, on the main menu, selectFile > Print Options.
- To open theWorkstations Optionsdialog box, on the main menu, selectTools > Options.
Configure font and color for items displayed in the editors or on Ladder or Structured Text reports using the
Ladder
and Structured Text
Editor/Listing Font/Color
categories.The name of the category visible in the options dialog varies depending on which options are being set, the display or print options. For
Workstation Options
, all categories refer to the Ladder or Structured Text Editor; for Print Options
, the categories refer to the Ladder Listing
or Structured Text Listing
.This table lists the configurable settings.
Setting | Description |
---|---|
Font | The font used for text in the editor. |
Size | The size of text in the editor. |
Items | The objects in the editor for which you can choose the color, such as comments, instructions, tags, and line numbers. |
Foreground color | The color of the foreground in the editor. |
Background color | The color of the background in the editor. |
Sample | A preview of the selected item with configured settings. |
Provide Feedback