Configure Sequential Function Chart routine execution

To configure sequential function chart routine execution:
  1. On the
    Online
    toolbar, select the
    Controller Properties
    icon.
  2. On the
    Controller Properties
    dialog box, select the
    SFC Execution
    tab.
  3. In the
    Execution Control
    section, choose from:
    • Execute current active steps only
    • Execute until FALSE transition
  4. In the
    Restart Position
    section, choose from:
    • Restart at most recently executed step
    • Restart at initial step
  5. In the
    Last Scan of Active Steps
    section, choose from:
    • Automatic reset
    • Programmatic reset
    • Don’t scan
  6. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.