Controller Properties - Advanced Time Sync dialog box
The
Advanced Time Sync
dialog box provides information related to the CIP Sync clocks in the network or in the local chassis. Use this dialog box to find out which device is currently regulating system time and to set local clock priorities.
TIP:
To open the Advanced Time Sync dialog:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click theDate/Timetab, and clickAdvanced.
When the controller is offline or Time Synchronization is unavailable, all fields except CIP Sync Time Synchronization and priority fields are blank. The priority fields and Time Synchronization state are available when the controller is offline or online.
For more information about CIP Sync and time synchronization, refer to , publication IA-AT003.
Integrated Architecture
and CIP Sync Configuration Application Techniques
IMPORTANT:
Information about the clocks is not displayed if offline or if Time Synchronization is unavailable.
Provide Feedback