Controller Properties dialog box - Network tab
Use the
Network
tab on the Controller Properties
dialog box to configure settings and monitor faults for a Device-Linked Ring (DLR) topology. The Network
tab is only available for controllers with an embedded Ethernet port.
TIP:
To open the Controller Properties dialog box - Network tab:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click theNetworktab.
The settings on the
Network
tab are available when:- Online.
- User has security permissions to edit the controller settings.
- The controller is not operating in Hard Run mode.
For more information on how to configure network properties, refer to the EtherNet/IP Embedded Switch Technology Application Guide publication ENET-AP005.
Provide Feedback