Controller Properties dialog box - Security tab parameters

Controller Properties dialog box - Security tab parameters

Use the
Security
tab of the
Controller Properties
dialog box to configure security settings for the controller. The table describes the parameters on the
Security
tab. Some settings on the
Security
tab are not available for all controller types and some require
FactoryTalk Services Platform
version 2.50 (Service Release 5) or later.
Setting
Description
Requirements
Security Authority
The
FactoryTalk
directory used to secure the project.
If it is available, may also display a Unique Resource Identifier (URI). The URI is the name of the computer that is hosting the
FactoryTalk
Network Directory used to secure the project. For example, the Security Authority list might display:
FactoryTalk Security
<ComputerName>.
This setting is enabled when permission is set to
Allow
for Product Policy
RSLogix5000\Controller: Secure
. The
FactoryTalk Security
settings are configured in the
FactoryTalk Administration Console
in the
FactoryTalk
Network Directory.
Use only the selected Security Authority for Authentication and Authorization
This check box associates the project with a specific security authority. Select the check box to require users interacting with this project to be authenticated and authorized by the selected security authority. The security authority identifier must match.
When associating a project with a specific security authority, it is associating the project with a specific
FactoryTalk
Network Directory that is identified by a security authority identifier. Projects that are secured and bound to a specific security authority cannot be recovered if the security authority identifier of the
FactoryTalk
Network Directory used to secure the project no longer exists. Otherwise, unauthenticated users must rely on Guest User permissions.
IMPORTANT:
Before associating this project with a specific security authority,
Rockwell Automation
recommends backing up the
FactoryTalk Directory
and saving unsecured versions of this project file in .ACD, .L5X, or .L5K formats in a secure location.
TIP:
When selecting this check box, Guest User permissions are cached within the project. The
Logix Designer
application uses Guest User
permissions when the project is opened but not connected to the
FactoryTalk
Security Authority that secures the project. By default, all Guest User permissions are denied. Guest User permissions are configured in the
FactoryTalk Services Platform
.
This check box is not available when:
  • No Protection
    is the selected Security Authority.
  • FactoryTalk Services Platform
    is not version 2.50 (Service Release 5) or later.
  • The user does not have security permissions to secure a project.
Secure With
Select a
Secure With
option:
  • To associate the project with a Logical Name in
    FactoryTalk Services Platform
    , select
    Logical Name
    <Controller Name>
    . If there is no existing Logical Name that matches the controller name, the
    Logix Designer
    creates a new Logical Name with the controller's name and it inherits permissions from its parent resource.
  • To associate the project with a Permission Set configured in
    FactoryTalk Services Platform
    , select
    Permission Set
    and select a permission set from the list.
The listed permission sets are maintained using the
FactoryTalk Administration Console
and are used to identify a set of actions that are allowed or denied for a particular user and computer combination.
None
Restrict Communications Except Through Selected Slots
Select this check box to restrict communications through any slot that is not trusted. Only the slots selected under
Select Slots
are trusted communication paths for the controller. Clear the check box to allow the controller to communicate without communication restrictions.
IMPORTANT:
When this check box is selected, communications are restricted through USB or serial ports and firmware updates are restricted to trusted slots when using AutoFlash or
ControlFLASH
. Support is restricted for tools that require access to restricted data through class 3 connections. .
For more information about communication paths and trusted slots, see
Failed to go online with the controller > Communications path not trusted by the controller
.
Failed to go online with the controller > Communications path not trusted by the controller
Trusted slots are required for these products and features:
  • Logix Designer
    application - to go online with the controller
  • FactoryTalk Alarms and Events
    and external data
  • RSLinx Classic
    or
    FactoryTalk Linx
    to communicate with the controller.
Tip:
This check box is only available on <CL> 5570 and 5580 controllers.
Select Slots
The
Select Slots
grid configures the trusted slots for the controller. When the
Restrict Communications Except Through Selected Slots
check box is selected, select at least one slot that is not occupied by the controller.
If the chassis size for the project is known, the number of slots equal to the chassis size are displayed in the dialog box. Otherwise, 17 slots (0-16) are displayed in the dialog box.
For more information about communication paths and trusted slots, see
Failed to go online with the controller > Communications path not trusted by the controller
.
Failed to go online with the controller > Communications path not trusted by the controller
None.
Enable Controller Embedded Web Page
Select to enable access to web pages that track controller, network, and backplane performance. Access is disabled by default.
The check box is only shown for controller types that support controller web pages.
The check box is disabled when online with the controller.
Enable Controller Embedded Web Page messages
When CIP Security overrides the web page setting and the overridden setting is different than the project setting, a red flag and this message is shown:
The web page setting is overridden by CIP Security and is different than the project setting.
When CIP Security overrides the web page setting and the overridden setting is the same as the project setting, this informational message is shown:
The web page setting is overridden by CIP Security and is the same as the project setting.
Shows the information icon when CIP Security is overriding the Controller Embedded Web Page setting and the overridden setting is the same as the project setting.
Shows a red flag warning icon when CIP Security is overriding the Controller Embedded Web Page setting and the overridden setting is different than the project setting.
When online with the controller, the message only shows when connected to a controller and CIP Security has the controller's web page setting configured.
Changes To Detect
Identifies the types of events that cause the
Audit Value
box to change. By default, all event types cause the
Audit Value
to change, resulting in a default value of: 0xFFFFFFFFFFFFFFFF.
Select
Configure
to open the
Configure Changes to Detect
dialog box to see a list of events that are monitored.
None.
Audit Value
A unique value generated when a project is downloaded to the controller or loaded from a storage device. This value is updated when an event occurs. Some events always cause an
Audit Value
change, while others are selectable in the
Configure Changes to Detect
dialog box. When the controller is offline, the
Audit Value
box is blank.
None.
Tracked State Value
A hexadecimal value that indicates the current state of tracked components. If a tracked component changes, the
Logix Designer
application updates this value to indicate that a component changed. When the controller is offline, this box is blank.
None.
View Components
Displays the
Tracked Components
dialog box.
None.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal