About permissions for Guest Users
When you configure permission sets and logical names in
FactoryTalk Administration Console
, you can also configure permissions for Guest Users. The permissions for Guest Users determine the level of access for users who are not authenticated on the same FactoryTalk
directory that the project was secured with.Permissions for Guest Users are cached in the project file to which they are associated. However, the permissions are only stored in the project file for permission sets that have been applied to objects by a user of the primary
FactoryTalk
directory. Refer to the
FactoryTalk
online help for more information on permissions for Guest Users.Provide Feedback