Program parameter description overview

Program parameter description overview

In a program parameter, you can provide a description. If you do not provide a description for a particular item, the description of the next highest item in the tag hierarchy appears in the
Description
column in the
Parameters
tab of the
Equipment Phase
Properties
dialog.
These rules determine the contents of the
Description
column if you do not provide a description:
  • If the item is an alias, the description of the base tag (if available) is used.
  • If the item is a tag identifier of a structure, the corresponding member description of the structure’s data type is used.
  • If no other descriptions can be found in the hierarchy, the description of the item’s data type is used.
If the description is dimmed in this column, the description originates from another item.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal