Routine Properties dialog box - General tab - Function Block Routine parameters
The
General
tab on the Routine Properties
dialog box lists the properties associated with the selected function block routine. The following table describes the parameters on the General
tab.Parameter | Description |
Name | The routine name, which must follow the Logix Designer application IEC-1131 Name Standard. |
Description | A description for the routine that contains a maximum of 512 characters. |
Type | The language type of the main logic in the routine: Ladder, Function Block Diagram, Sequential Function Chart, or Structured Text. |
In Program | The program to which the routine belongs. |
Number of sheets | The number of sheets contained in the routine. |
Permission Set | Applies a set of permissions that controls access based on the permissions configured in FactoryTalk Security . The default setting, <Controller Inherited> , applies the same security settings that have been applied to the controller or project. |
Provide Feedback