Failed to modify operand
Tried to modify the value of an operand or tag, but the operation failed. This could occur because:
- the operand does not contain a valid tag
- the tag is a structure of some type
- the value is not a valid value for the type of tag (for example, the value may not be a valid integer value for a SINT tag)
- the tag was deleted (for a program scoped tag)
Provide Feedback