Edit routine properties
Use the
Routine Properties
dialog box to edit routine properties.To edit routine properties:
- In theController Organizer, right-click the routine and selectPropertiesto open theRoutine Propertiesdialog box.
- InName, type a name for the routine.TIP:The state routine names for equipment phases are fixed and cannot be changed.
- InDescription, enter a description of the routine.
- To apply a set of permissions to the routine, select aPermission Set. The permission set controls access to the routine based on the permissions configured inFactoryTalk Administration Console. The default setting,<Controller Inherited>, applies the same security settings that have been applied to the controller or project.
- SelectOK.
Provide Feedback