PVSD HMI command buttons
Use the
Command configuration
tab on the PVSD Properties
dialog box to label the HMI command buttons for Process Variable Speed Drive (PVSD) instructions.To label HMI command buttons for PVSD instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select the arrow next toHMIand then selectCommand configuration.
- Set the parameters:
- Command button. Type the label to display on the command button. By default, label information appears, for example, start forward, start reverse, stop. Clearing the label information affects the information displayed on the command buttons in theGeneraltab. Images will appear with no text.
- Target state. Type the label to display for the target state, for example, Running, Forward, Running reverse, or Stopped.
- Transition state. Type the label to display for the transition state, for example, Starting forward, Starting reverse, or Stopping .
- View the read-only parameters:
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Stopped, Running, or Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Drive fault or I/O fault.
- SelectApply.
Provide Feedback