Reset counters for PRT instructions
Use the
General
tab of the PRT Properties
dialog box to monitor the instruction status and to reset the run time and start counters for Process Run Time and Start Counter (PRT) instructions.To reset the counters for Process Run Time and Start Counter (PRT) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- When online, use theClearbuttons:
- To clear the maximum, continuous runtime for any start, selectClear Max.
- To clear the total run time, selectClear Total.
- To clear the count of start attempts, selectClear Starts.
Provide Feedback