Print Options dialog box settings

Use the
Print Options
dialog box to customize the display format of your reports.
TIP:
If
FactoryTalk Security
is enabled, this dialog may be disabled, depending on the levels of access that have been defined. For details about
FactoryTalk Security
see
FactoryTalk
Help:
Start > Programs >
Rockwell Software
Rockwell Software
>
FactoryTalk
Tools >
FactoryTalk
Help
.
The following table describes the parameters available on this dialog box:
Parameter
Description
Categories
A list of all options categories that can be configured. Select a category and its options appear to the right of the list. When you change an option, an asterisk (*) is appended to the name of the category. You can change options from as many categories as you wish; select
Apply
or
OK
to apply options for any modified categories.
Reset Category
Select this button to return to the factory default settings for the selected category. Note that not all categories support this behavior; the button will be disabled if you select a category that does not support this behavior.
OK
Select this button to accept your changes and close the Print Options dialog.
Cancel
Select this button to cancel your changes.
Apply
Select this button to apply your changes and continue editing in the Print Options dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.