- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Add a Boolean action to a step
Divide each step into the actions that the step accomplishes, then add boolean actions to the step.
Boolean actions do not contain a text area for embedding structured text or calling other routines. Boolean actions may be converted to a non-boolean actions, if required.
To add boolean actions to each step
- Select the step in which the action executes.
- SelectBoolean Action
.
- InProperties, type a name for the action.
- Choose the scope for the tag of the action.
- SelectOK.
Provide Feedback