Set the priority of sequences on a selection branch

Set priority of sequences on a selection branch to change which sequences are evaluated first.
To set the priority of sequences on a selection branch
  1. Open Set Sequence Properties.
  2. Select either:
    • Select
      Use Default Priorities (left to right on routine)
      to evaluate sequences from left to right.
    • Clear
      Use Default Priorities (left to right on routine)
      to set priorities manually.
  3. If
    Use Default Priorities (left to right on routine)
    is cleared, set priorities manually:
    1. In
      Set Sequence Properties
      , select a sequence from the list.
    2. Use the Up and Down buttons to change the relative position of the selected sequence.
      Actions higher in the list are evaluated before actions lower in the list.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.