- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Edit SBR/RET properties
Edit SBR/RET properties to pass and return parameters to and from a sequential function chart routine when calling it through a JSR instruction.
To edit SBR/RET properties
- Enter or modify the input parameters, as appropriate.
- Enter or modify the return parameters, as appropriate.
- ClickOKto apply edits and close the SBR/RET Properties dialog.
Provide Feedback