- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Create a button that shuts down the host system
Add a button that shuts down the host operating system on which the
FactoryTalk Optix Application
runs.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing Shut down system
immediately shuts down your Windows system.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select , and enterShutDownSystemButton.
- InProperties, setTexttoSHUT DOWN HOST SYSTEM.
- InEvents, next toMouseClick event, select and select .
Provide Feedback