Add NuGet packages

Add NuGet packages

Some
FactoryTalk Optix Studio
library widgets and scripts require specific NuGet packages to be installed.
For more information about NuGet, see What is NuGet and what does it do? | Microsoft Docs.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 2.0 destination framework.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.