Module log level configuration
Configure the module log level to change the maximum level of information displayed in the
Output
panel.By default, the
FactoryTalk Optix Studio
Output
panel shows all message types: warning, error of minimum severity, error of maximum severity, and other detailed information .You can change the maximum level of information displayed in the panel, either for all FactoryTalk Optix Studio
Platform modules, or for specific modules.
TIP:
All information is stored in the system log file, regardless of the maximum information level displayed in
FactoryTalk Optix Studio
.Provide Feedback