Select a client device

Select a client device

Select an already configured target client device to deploy
FactoryTalk Optix Applications
over the network to the client device.
  1. From the main toolbar, next to
    Run
    Run
    , select the target client device drop-down.
  2. (optional) In
    Client device settings
    , to display only the active remote client devices, toggle Active remote devices.
    TIP: Refresh remote client devices by selecting Refresh.
  3. Select a client device.
  4. Click
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal