Copy a graphic object

Copy a graphic object

Copy a graphic object to duplicate the configuration of the graphic object. Copied graphic objects create consistency and save time when creating graphic objects.
  1. In
    Project view
    or in the window, select the container or graphic object.
  2. Right-click the graphic object and select
    Copy
    or press
    CTRL+C
    .
  3. Right-click in
    Project
    view
    or the window and select
    Paste
    or press
    CTRL+V
    . The graphic element is pasted on top of the copied graphic element.
  4. Drag the new graphic object off the copied graphic object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal