Create a Presentation Engine

Create a Presentation Engine

Add a Native Presentation Engine or a Web Presentation Engine to your project.
TIP: Each
FactoryTalk Optix Studio
project can contain a single Native Presentation Engine and a single Web Presentation Engine.
  1. In
    Project view
    , right-click a window object.
  2. Select one of the following options:
    • To create a default Presentation Engine, select
      New
      Native Presentation Engine
      .
    • To create a Web Presentation Engine, select
      New
      Web Presentation Engine
      .
  3. In
    Properties
    , set any required Presentation Engine properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal