Resize the window

Resize the window

Set the size of the window object of the to specify the size of the Design Area.
  1. In
    Project view
    , select the window object.
  2. In
    Properties
    , in
    Height
    , enter the value for the height of the window.
  3. In
    Width
    , enter the value for the width of the window.
  4. (optional) In
    Full Screen
    select
    True
    to automatically make the user interface the same size of as the screen at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal