- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Push Agent properties
Configure Push Agent properties to send data to the cloud using MQTT.
Property name | Property type | Property description |
---|---|---|
DataLogger | NodeId | A reference to the data logger instance. |
PushFullSample | Boolean | If True , the transfer mode is used. If False , the transfer mode is used. |
PreserveDataLoggerHistory | Boolean | If True , the data is sent and historicized.If False , every time the data is transferred to the auxiliary store, the data is deleted from the data logger. |
MaximumStoreCapacity | Int32 | The maximum capacity of the auxiliary store used by the Push Agent. |
MaximumItemsPerPacket | Int32 | The number of records encapsulated in a packet. transfer mode sends only one line per packet.
TIP:
When
PushFullSample is set to True , set the MaximumItemsPerPacket to 1 . |
MaximumPublishTime | Duration | The maximum time interval after which data is taken from the auxiliary store and sent to the cloud. The interval is used when there are at most MaximumItemsPerPacket records in the auxiliary store. |
MinimumPublishTime | Duration | The minimum time interval after which data is taken from the auxiliary store and sent to the cloud. This interval is used when there are at least MaximumItemsPerPacket records in the auxiliary store. You may want to increase the sending frequency to download the queue of the store. |
ClientId | String | The ID of the client that has to send the data. |
BrokerIPAddress | String | The broker IP address. |
BrokerPort | Int32 | The broker port (if you want to communicate with SSL, set the value to 8883 ). |
BrokerTopic | String | The name of the topic you want to publish on preceded by / .For example, if the broker topic is /custom_topic , the BrokerTopic parameter is custom_topic . |
QoS | Int32 | The Quality Of Service (QoS) level used to send information.
|
UseSSL | Boolean | Enables or disables secure communication.
|
Username | String | The username for authenticated communication with the broker. |
Password | Password | The password for authenticated communication with the broker. |
Provide Feedback