Navigate a trend chart
Navigate the X axis and Y axis of a trend chart.
- Select a point and drag it horizontally to navigate the X axis.TIP: If theFollowproperty is set toTrue, it stops when you interact with the graph. To restart the automatic scrolling of the X axis, move along the X axis to the current instance.
- Select a point and drag it vertically to navigate the Y axis.
- Select a pointer and drag it diagonally to browse on both axes.
Provide Feedback