- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Change the user authentication mode
Change the default user authentication mode for the project to allow local
Windows®
users and Active Directory users to log into the FactoryTalk Optix Application
.
IMPORTANT:
If you use the Active Directory user authentication mode, the groups associated with the users are queried by Active Directory and mapped with the existing groups in
Project view
. For example:- A user belongs to a group in the model.
- The same group exists in Active Directory.
- In Active Directory, the user does not belong to the group.
- The user is removed from the group in the model.
- InProject viewpane, select the project node.
- InProperties, inAuthentication mode, select the authentication type that allows specific users to log in:
- Model only. Users created inFactoryTalk Optix Studio.
- Local only. LocalWindowsusers.
- Domain only. Active Directory users.
- Domain and local. Active Directory and localWindowsusers.
- Any. Users of any type.
- Select
Save.
Provide Feedback