Lock graphic objects protected with a password
Lock a password-protected graphic object to prevent other
FactoryTalk Optix Studio
users from editing child objects of the protected object.- InProject viewor in theEditor, next to the object to lock, select.
In
appears next to the password protected object. The child objects are hidden in
Project view
and in the Editor
, ![](/content/dam/dita/en/factorytalk-optix/current/_images/password-protected-locked.png/_jcr_content/renditions/original)
Project view
and cannot be edited.Provide Feedback