Add a screen type

Create a Screen type in the
Screens
folder.
Prerequisites
  1. In
    Project view
    , right-click
    Screens
    and select
    New
    Screen
    .
  2. (optional) In
    Properties
    , set the screen type properties.
    TIP:
    By default, each new screen stretches to cover the entire parent object.
    For more information, hover-over the properties.
    Each instance of the screen type uses these properties as default properties.
  3. (optional) Add objects to the screen type.
    Each instance of the screen type includes the children objects of the screen type. You cannot remove objects inherited by screen instances from screen types.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.