- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Open an object
Open an object from
Project view
.- InProject view, double-click the object or mouse over the object and then select.
The object opens in a separate tab if the object has a dedicated editor.
Properties
for the object also open.Provide Feedback