Develop a color-coded alarm dashboard
Create a multilingual interface that displays color-coded alarms and enables you to acknowledge and confirm them.
Application example
![](/content/dam/dita/en/factorytalk-optix/current/_images/ColorCOdedAlarmsDashboard.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
ColorCodedAlarmGrid.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
![](/content/dam/dita/en/factorytalk-optix/current/_images/ColorCodedAlarmGridDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback