Add users (server)

Create multilingual users.
Prerequisites
  1. To add users
  2. Create a folder for domain users:
    1. In
      Project view
      , expand
      Security
      .
    2. Right-click the
      Users
      folder and select
      New
      Folder
      .
    3. Hover-over the folder, select
      Edit
      , and enter
      DomainUsers
      .
  3. Create the domain users:
    1. Create two users by right-clicking
      DomainUsers
      and selecting
      New
      All
      Security
      Users
      User
      .
    2. Rename the users by hovering-over each user, selecting
      Edit
      , and entering:
      • Alice
      • Frank
    3. In
      Project view
      , select
      Alice
      .
    4. In
      Properties
      , set
      Locale
      to
      en-US
      .
    5. In
      Project view
      , select
      Frank
      .
    6. In
      Properties
      , set the
      Locale
      to
      it-IT
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.