Develop a filterable list box
Develop a list box filled with random strings that you can filter by entering text into a filter text box.
Application example
![](/content/dam/dita/en/factorytalk-optix/current/_images/FilterableListBoxExample.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
FilterableListBox.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
![](/content/dam/dita/en/factorytalk-optix/current/_images/FilterableListBoxDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback