Allocate a FactoryTalk Optix Studio Pro entitlement to your organization
A newly purchased entitlement can be viewed by the purchaser in FactoryTalk Hub. Then, the entitlement must be allocated to the related organization, to be made available to other users as well.
- Access FactoryTalkHub.com to view your new entitlement.
- In the FactoryTalk Hub page title bar, select
, then select
View Entitlements.The new entitlement appears at the top ofAll entitlementsunderAvailable for allocation. - Verify that the correct organization name appears on the right side of the FactoryTalk Hub title bar.
- Locate the entitlement that you want to assign to your organization and selectAllocatenext to the entitlement row.
- Ensure that the entitlement, organization and allocated entitlements quantity are correct, then selectReview Allocation.TIP: Once allocated to an organization, an entitlement cannot be deallocated.
- When prompted, confirm the allocation.The entitlement is allocated to the organization.
- In the upper left corner of the FactoryTalk Hub web page, selectHome.
- Select theFactoryTalk Optixtile.
- Authenticate as required.
- At the top of the FactoryTalk Optix landing page, selectEntitlements.
- On theEntitlementspage, selectOrganization entitlements.
The allocated entitlement appears.
Provide Feedback