Device registration to a domain
You must register a device to a domain before continuing with its configuration process.
The device registration procedure might differ, based on the firmware version of the device that you want to register.
If your device is a
Stratix 4300
, proceed as follows:®
featuring a firmware version older than or equal to 4.0.2- Access the FactoryTalk Remote Access Manager and select.
- Select the domain folder in which you want to register your device.
- Select thecircled plusicon
- SelectAdd device.
- SelectAdd device locally.
- In theAdd device locallydialog window, enter the device user name and password.. A list displays the MAC addresses of the devices found on your network.NOTE: These credentials are the same that you use to access the device System Manager.
- Select the device that you want to add to your domain.
- Enter a device name in theInitial namefield.
- SelectRegister.NOTE: You might be prompted to log in to your account, if you have not done it yet.
- See Device Setup to configure your device.
If your device is one of the following:
- Stratix 4300®featuring a firmware version newer than 4.0.2
- OptixPanel™featuring a firmware version 4.0.4 or newer
- Embedded Egde Compute Module featuring a firmware version 4.0.4 or newer
proceed as follows:
- Access the FactoryTalk Remote Access Manager and select.
- Select the domain folder in which you want to register your device.
- Select thecircled plusicon
- SelectAdd device.
- SelectAdd device remotely.
- In theAdd devicedialog window, enter the device ID and password.
- SelectSave. The newly registered device is named<No name>in the previously selected folder and must be renamed.
- Rename the device.
- See Device Setup to configure your device.
Provide Feedback