Delete a routine from the organizers

Use the
Delete
command to remove a routine from the
Controller Organizer
and the
Logical Organizer
. Deleting a routine from either organizer also deletes it from the other organizer. You can delete only one routine at a time.
There are no restrictions to this operation when the system is offline.
When the system is online, you cannot delete a routine if:
  • The controller is in
    Remote Test
    or
    Remote Run
    and the routine is the Main, Fault, Prestate (equipment phase), or State (equipment) routine.
  • The routine is referenced by a Jump to Subroutine (JSR) instruction.
    TIP: If FactoryTalk Security is enabled, FactoryTalk Security permissions are required to create and delete items in the
    Controller Organizer
    and the
    Logical Organizer
    .
To delete a routine
:
  1. Right-click the routine, and then choose
    Delete
    .
  2. Choose
    Yes
    to confirm the deletion.
    TIP:
    You can also delete a routine by selecting it and then using one of these methods:
    • From the
      Menu
      bar, select
      Edit
      >
      Delete
      .
    • Press the
      Delete
      key.
For more information about the organizers, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.