Controller Properties dialog box - Capacity tab settings for 5x80 controllers

Controller Properties dialog box - Capacity tab settings for 5x80 controllers

The
Capacity
tab of the
Controller Properties
dialog box shows the number of used and unused blocks for the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370, and
GuardLogix
5570 controllers
. Blocks represent units that consume the controller’s memory. Although block sizes are not physically equivalent to the bytes measured in previous 5570 controllers, in general, applications that fit in a specific controller with divided memory should fit in the same controller with one common memory area.
If the size of the project exceeds the capacity available in the controller, a message appears that states the overage size in blocks. When the used blocks exceed the available blocks, the project cannot be downloaded to the controller.
Settings that do not apply to the controller are hidden.
The ability to change the settings on this tab can be controlled by
FactoryTalk Security
permissions.
Parameter
Description
Capacity (Standard Capacity)
The total number of blocks in standard memory available and used by the project.
TIP:
If the controller is a Standard controller, the parameter appears as
Capacity
. If the controller is a Safety controller, the parameter appears as
Standard Capacity
.
Safety Capacity
The total number of blocks in safety memory available and used by the project for safety components such as safety task, safety programs, safety routines, safety Add-On Instructions, safety tags, and safety task signature.
This is available only for Safety controllers.
Total
Shows the total number of blocks available in the controller.
Available
Shows the number of unused blocks. The available capacity is graphed in white on the slider.
Used
Shows the number of blocks used by the project. The used blocks are graphed in gray on the slider.
Ethernet Nodes
Shows information about the Ethernet nodes connected to the controller.
  • Maximum/Recommended Maximum
    - Number of Ethernet nodes supported by the controller, or the recommended maximum number of Ethernet nodes for the controller.
    • Used -
      Current number Ethernet nodes in the I/O Configuration tree
      If the controller is offline, L5k_node exceed limit icon appears next to the
      Used
      parameter when the node count exceeds the limit.
      For controllers that do not limit the number of Ethernet nodes, L5K_node_yellowcautionicon appears next to the
      Used
      parameter when the node count exceeds the recommended limit and this message appears:
      The recommended node limit has been exceeded. It may be possible to connect additional nodes depending on the node type and system architecture.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal